Single-wire SCI mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Single-wire SCI mode

2,662 Views
kosthala
Contributor I
Hello,

In our application we use the MC9S08AW32 and we try to use the single wire mode of SCI.
The code to initialize the SCI is:

      mov    #$A0, SCI1C1
      mov    #$00, SCI1C3
      mov    #$24, SCI1C2    ; enable RECEIVER
      cli

but the SCI is not working. The transmiter is sending data but the
receiver doesn't receive any data at all.
Is there something else we need to know in order to make it work?

Thanks in advance.



Labels (1)
0 Kudos
Reply
2 Replies

1,800 Views
bigmac
Specialist III
Hello,
 
For single wire transmit/receive operation, It would be usual to have both transmitter and receiver sections of the SCI enabled - for this the value for SCI1C2 register would need to be $2C.  Otherwise, there is little point in selecting-single wire mode for a receive only application.
 
Additionally, the TXDIR bit within SCI1C3 would need to be set to 1 whenever a byte is sent, and then returned to 0, once the transmission is complete, ready to receive any incoming data.
 
Regards,
Mac
 

Message Edited by bigmac on 2007-04-0612:09 AM

0 Kudos
Reply

1,800 Views
kosthala
Contributor I
Hello Mac,

Sorry for the delayed answer (i was away from civilization for a few days). Anyway, your solution was
perfect   :smileyhappy:
Thank you very much.
0 Kudos
Reply