Single Board Computer with the HCS08

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Single Board Computer with the HCS08

3,263 Views
FC
Contributor III
Hello,
 
I am need of a single board computer with an HCS08 MCU that is ready to be used in the end application.  Are there any companies that produce them?
 
Thanks
Labels (1)
0 Kudos
Reply
2 Replies

1,526 Views
glork
Contributor I
Hello FC.
I have a small company that produces a board based on the MC9S08GB60 (HCS08). It can be had either "bare-bones" or pre-configured with some buffered I/O. It also has an RS-232 port and on-board regulator, etc.
Go to http://gadgetwerksinc.com for a picture and details. Freescale forum members get an un-official 20% discount off the list price.
ron
0 Kudos
Reply

1,526 Views
Jaux
Contributor I

We have developed a simple single-board MCU based on the MC9SAW60CFUE

Features:

. Integrated switching supply, 9-20 VAC input
. AW60 is 5V based
. 24-key keyboard interface ( 8 KBI x 3 scan, active low )
. LCD interface
. RS-485 interface
. All of the GPIO pins are routed to edge pin connectors
. BDM Interface

As a fanatic Freescale junkie, and because you have a small company ( we were all small once), I will let you have the schematics, Gerbers, etc. which you will need to construct the board free of charge.

I am in a good mood, and is Xmas anyway - I will even let you have a blank PCB which you can use to construct the MCU.

See pics attached.

Let me know if you want it.

John Ulyate

RIMG0004.jpg

RIMG0005.jpg

Message Edited by t.dowe on 2009-10-20 01:37 PM
0 Kudos
Reply