Setting 115200baud on QE128 using internal oscillator

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Setting 115200baud on QE128 using internal oscillator

2,374件の閲覧回数
abhijit_78
Contributor I
Hi,
 
I need to set 115200bps on my QE128 board using internal oscillator. I am using processor expert to generate the code and have set internal oscillator freq to 36KHZ to get a bus clock of 9.216MHZ which can then easilty generate the required baud rate of 115200.
 
However, the actual bus clock that i get is 8.35MHZ and hence the baud rate is also not correct.
 
Pls suggest.
 
Thanks.
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,436件の閲覧回数
ProcessorExpert
Senior Contributor III
Your problem has been solved here:

http://forums.freescale.com/freescale/board/message?board.id=CFCOMM&message.id=4376#M4376


best regards
Vojtech Filip
Processor Expert Support Team UNIS

www.processorexpert.com
0 件の賞賛
返信

1,436件の閲覧回数
abhijit_78
Contributor I
Thanks for the information.
 
I am now able to communicate at 115200baud.
0 件の賞賛
返信