Serial communications Approach

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Serial communications Approach

跳至解决方案
2,354 次查看
karthick1987
Contributor II

 

I had to fiddle around with the SCI a bit and  wanted to know something.

 

This is what my serial code looks like (I am not using interrupts here).

       
       while(SCI1S1_TC == 1)
       {
       }

 

SCI1D = i;              
while(SCI1S1_TC == 1)      

{       }

 

and in the main for loop i have

 

 

for( ; ; ) 

  {       

          LCD_write('y');

          LCD_write('o');

    

    /* __RESET_WATCHDOG(); by default, COP is disabled with device init. When enabling, also reset the watchdog. */

  } /* loop forever */

 

LCD_write() is the function that contains the first piece of code.

 

Now I did notice on the LCD screen that it displayed a series of y's followed by a series of o's ! as opposed to series of yo's continuously !

 

This has led me to think that I am using the wrong approach to serial communication here. So please tell me if i am actually missing something out ? like the transmit buffer or something of that sort. Also I wanted to know what your approach to this would be like?

 

Please advice.

 

Cheers

Karthick

标签 (1)
0 项奖励
回复
1 解答
1,824 次查看
peg
Senior Contributor IV

Hello Karthick,

 

Your test here is wrong. The TC bit is set when the whole byte has been shifted out of the shift register. It is reset by reading it then writing to the SCID (amongst other more complicated things).

Normally you would test the TDRE bit for 1 before you write to SCID. With RS-232 you don't really care when the byte is completely shifted out.

 

It is normally used with, say, half duplex two-wire RS-485 where you need to know this to turn of the transmitter so you can recieve again. It is only tested after the last byte in a string of data has been written. The TDRE test above is still done between every byte of the string.

 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,825 次查看
peg
Senior Contributor IV

Hello Karthick,

 

Your test here is wrong. The TC bit is set when the whole byte has been shifted out of the shift register. It is reset by reading it then writing to the SCID (amongst other more complicated things).

Normally you would test the TDRE bit for 1 before you write to SCID. With RS-232 you don't really care when the byte is completely shifted out.

 

It is normally used with, say, half duplex two-wire RS-485 where you need to know this to turn of the transmitter so you can recieve again. It is only tested after the last byte in a string of data has been written. The TDRE test above is still done between every byte of the string.

 

0 项奖励
回复
1,824 次查看
karthick1987
Contributor II

Got it Peg

 

Thanks a lot mate. Its working now!

 

Cheers

Karthick

0 项奖励
回复