Sending command from MC9S08QE128

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Sending command from MC9S08QE128

4,056 Views
shumpi55
Contributor I
I want to send a command like C:\YahooMessenger.exe from MC9S08QE128 micro-controller .
Can anyone help me out?

Labels (1)
0 Kudos
Reply
5 Replies

2,710 Views
JimDon
Senior Contributor III
Send it to who? Using what?

0 Kudos
Reply

2,710 Views
shumpi55
Contributor I
I want to send the command c:\yahoomessenger.exe via serial cable(RS232) from MC9S08QE128 micro-controller to the PC so that as soon this command reaches the PC it opens yahoo messenger.
0 Kudos
Reply

2,710 Views
JimDon
Senior Contributor III

Well, you are going to need a program running on the PC that reads the serial port and runs the command when you send it.

You might be able to find a terminal program that has a scripting language that would do that, or you could write it.



0 Kudos
Reply

2,710 Views
shumpi55
Contributor I
thanks

0 Kudos
Reply

2,710 Views
J2MEJediMaster
Specialist I
Topic police says: Please don't cross-post into the forums! I'll leave this one here, but the other is deleted.

---Tom
0 Kudos
Reply