Sending command from MC9S08QE128

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Sending command from MC9S08QE128

3,113 次查看
shumpi55
Contributor I
I want to send a command like C:\YahooMessenger.exe from MC9S08QE128 micro-controller .
Can anyone help me out?

标签 (1)
0 项奖励
回复
5 回复数

1,767 次查看
JimDon
Senior Contributor III
Send it to who? Using what?

0 项奖励
回复

1,767 次查看
shumpi55
Contributor I
I want to send the command c:\yahoomessenger.exe via serial cable(RS232) from MC9S08QE128 micro-controller to the PC so that as soon this command reaches the PC it opens yahoo messenger.
0 项奖励
回复

1,767 次查看
JimDon
Senior Contributor III

Well, you are going to need a program running on the PC that reads the serial port and runs the command when you send it.

You might be able to find a terminal program that has a scripting language that would do that, or you could write it.



0 项奖励
回复

1,767 次查看
shumpi55
Contributor I
thanks

0 项奖励
回复

1,767 次查看
J2MEJediMaster
Specialist I
Topic police says: Please don't cross-post into the forums! I'll leave this one here, but the other is deleted.

---Tom
0 项奖励
回复