Sending command from MC9S08QE128

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Sending command from MC9S08QE128

4,081件の閲覧回数
shumpi55
Contributor I
I want to send a command like C:\YahooMessenger.exe from MC9S08QE128 micro-controller .
Can anyone help me out?

ラベル(1)
0 件の賞賛
返信
5 返答(返信)

2,735件の閲覧回数
JimDon
Senior Contributor III
Send it to who? Using what?

0 件の賞賛
返信

2,735件の閲覧回数
shumpi55
Contributor I
I want to send the command c:\yahoomessenger.exe via serial cable(RS232) from MC9S08QE128 micro-controller to the PC so that as soon this command reaches the PC it opens yahoo messenger.
0 件の賞賛
返信

2,735件の閲覧回数
JimDon
Senior Contributor III

Well, you are going to need a program running on the PC that reads the serial port and runs the command when you send it.

You might be able to find a terminal program that has a scripting language that would do that, or you could write it.



0 件の賞賛
返信

2,735件の閲覧回数
shumpi55
Contributor I
thanks

0 件の賞賛
返信

2,735件の閲覧回数
J2MEJediMaster
Specialist I
Topic police says: Please don't cross-post into the forums! I'll leave this one here, but the other is deleted.

---Tom
0 件の賞賛
返信