SPI data storage for sensors

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SPI data storage for sensors

3,758件の閲覧回数
nanoampgary
Contributor I

I am looking for design examples using the MC9S08  to  store data from sensors in external serial SPI Flash or EEprom. I also need referrals to consultants who could adapt the code to store data in 64K serial SRAM for the MC9S08 /Serial SRAM demo board we are designing
Gary

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,666件の閲覧回数
rhinoceroshead
Contributor I

I couldn't help noticing that your area code is Minneapolis/St. Paul - which is where I'm at.  What you're asking sounds simple enough.  Feel free to send me a message with more details.  Which microcontroller, Flash and SRAM chips are you using?  Is the code written in assembler or C?

0 件の賞賛
返信

1,666件の閲覧回数
nanoampgary
Contributor I
Here is our prfereence
processor MC9S08QG
Code in C
265 K SPI serial SRAM
Call me 651-439-1993
0 件の賞賛
返信