SMAC problem with NCB board - have yu experienced the same?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SMAC problem with NCB board - have yu experienced the same?

2,531件の閲覧回数
zoz
Contributor I
I am trying to use SMAC demo applications on NCB boards: Repeater, Lighting demo(controller and device). Lighting demo - controller works good (transmitting messages ok).
But neither the lighting device nor the repeater application receives properly! The repeater sometimes receives a packet but very rarely and the received data is not correct.
I have tried BeeStack CodeBase and MAC Codebase applications as well on the same boards and they all worked perfectly - so the boards are good.
I have tried SMAC demo appliactions on SARD boards as well and they all performed good!
 
So I presume there is something wrong in the SMAC codebase when it is applied to NCB boards. The problem is with receiving, the transmitting works perfectly.
 
Have you experienced the same problem??
ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,259件の閲覧回数
zoz
Contributor I
The problem only occurs in promiscous mode... but why?
0 件の賞賛
返信

1,259件の閲覧回数
Alex_RUS
Contributor I
I am sorry.
Could you say in couple of words what is "promiscous" mode. What means "promiscous"?? Thank you.
0 件の賞賛
返信

1,259件の閲覧回数
peg
Senior Contributor IV
Hi,
 
Promiscuous:
1. having an indiscriminate number of casual sexual relationships.
2. Lacking order.
 
I will leave it to you to apply it to SMAC.
It was spelt wrongly before.
 
0 件の賞賛
返信