SMAC in MC9S08QG8

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SMAC in MC9S08QG8

2,224 次查看
facundomaldonad
Contributor I
What I have to do to use SMAC with a MC9S08QG8? (if the supported MCU in BeeKit are MC68HCS08GT60, MC68HCS08GB60 and MC9S08QE128)

What pins I have to connect between the MC9S08QG8 and the MC13192?

Thanks!
标签 (1)
0 项奖励
回复
3 回复数

1,216 次查看
kanu
Contributor I
me also new in hcs08's, SO if anything incorrect then plz others correct that.

Peg is very correct.

ram and flash resources.for MC9S08QG8 are 512 bytes and 8K .
and required for smac are 2.5K-3K. so that can be implemented.
connections are throughfour wire SPI connections,as

MODEM MCU

MOSI-----MOSI
MISO----->MISO
M_IRQ---->IRQ
SPICLK---SPICLK

REGARDS..
KARAN.
0 项奖励
回复

1,216 次查看
bigmac
Specialist III
Hello, and welcome to the forum.
 
What flash and RAM resources are required to support SMAC?  I suspect that the 'QG8 would be too small.
 
Regards,
Mac
 


Message Edited by bigmac on 2008-10-21 09:39 AM
0 项奖励
回复

1,216 次查看
peg
Senior Contributor IV
Hi,

You can actually implement SMAC in devices as small as a QG4. No bells and whistles here though.
See this document. This was prior to beekit.
I suspect that the automation inherent in beekit may have introduced inefficiencies that may now preclude the QG, but you can definitely do it the old way with just SMAC. (sans B&W)
As far as the connections go, they would be pretty much the same (the same named pins MISO, MOSI etc)



Message Edited by peg on 2008-10-21 06:39 PM
0 项奖励
回复