SMAC and BeeStack together

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SMAC and BeeStack together

2,580 次查看
Rafael_21
Contributor I
Is it  possible to connect a SMAC device to a Beestack device?

Is it transparent to me? Or I need to program something?

thank you!
标签 (1)
0 项奖励
回复
2 回复数

1,536 次查看
NLFSJ
Contributor III
Hi
 
SMAC devices cannot directly connect to a ZigBee Network as they have different networking layers.  The only way to do this is via a gateway device that will do translation from one network to the other. 
 
    
 
 
 
 
Regards,
Nina
0 项奖励
回复

1,536 次查看
Mads
Contributor V
Hi,
SMAC is NOT compliant with 802.15.4 which ZigBee is build on top.
the SMAC is not compliant with the very strict timing and SMAC does not provide the acknowlegdement scheme as 802.15.4
 
Br,
Mads
0 项奖励
回复