SMAC and BeeStack together

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SMAC and BeeStack together

2,531 Views
Rafael_21
Contributor I
Is it  possible to connect a SMAC device to a Beestack device?

Is it transparent to me? Or I need to program something?

thank you!
Labels (1)
0 Kudos
Reply
2 Replies

1,487 Views
NLFSJ
Contributor III
Hi
 
SMAC devices cannot directly connect to a ZigBee Network as they have different networking layers.  The only way to do this is via a gateway device that will do translation from one network to the other. 
 
    
 
 
 
 
Regards,
Nina
0 Kudos
Reply

1,487 Views
Mads
Contributor V
Hi,
SMAC is NOT compliant with 802.15.4 which ZigBee is build on top.
the SMAC is not compliant with the very strict timing and SMAC does not provide the acknowlegdement scheme as 802.15.4
 
Br,
Mads
0 Kudos
Reply