SMAC 4.1 installation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SMAC 4.1 installation

3,010 Views
martyseb63
Contributor I
Hello,

I use codewarrior SE which is a limited version and a MCS08GT60.
I want to use smac 4.1 for zigbee's communication and I have some problems. When I want to compile smac, an error message appear and tell the size of file simple_phy is too high.
Then when I want to include smac to my projet there ara others problems : the file number is limited at 32. If I don't include all files, I have several problem of linker at the compilation.

Can you tell me how I can install and use SMAC 4.1

Thank
Labels (1)
0 Kudos
Reply
2 Replies

1,402 Views
stevasway
Contributor III
Hi,
why do you want to re-compile the SMAC?

It's better to use a demo project (like SimpleNetwork) which uses the lib, so you have less problems.

I used the SMAC4.1 in a project and it's ok. There are any particular problems about installing SMAC.

Try to modify for your purposes the existing projects.

Bye
Stevasway
0 Kudos
Reply

1,402 Views
AlanCollins
Contributor V

I strongly recommend you to get the latest SMAC codebase from BeeKit installer: www.freescale.com/zigbee

The SMAC you have is very old.

0 Kudos
Reply