SBC CAN MC33905 CAN_H/L Signal issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SBC CAN MC33905 CAN_H/L Signal issue

1,092件の閲覧回数
andrew_wu
Contributor I

SBC CAN MC33905 CAN_H/L signal rising and falling edges abnormal(The picture attached). It is not smooth but step in rising and falling edges. The step frequency is related to CAN slew rate. In Fast slew rate, the step frequency is about 100MHz and in Slow slew rate, the step frequency changed to about 25MHz. These steps on the rising and falling edges will cause EMC fail.

0 件の賞賛
返信
0 返答(返信)