SARD 13192

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SARD 13192

7,646件の閲覧回数
Diego
Contributor I
HEllo Everybody
 
I am working with a 13192 SARD.
I am working with codewarrior, and I was able to make my first programm using the wizard. (a simple program using leds).
 
Now I need to use the transceiver mc13192 to send data to another sard13192.
 
I want to implementate a Wireless UART.
 
But i do not know how to begin.
 
There are some libraries to manage the mc13192, or i have to implementate all from scratch??
 
How to begin with the modem mc13192??.
 
Do you have some example, source code??
 
Thanks
[email protected]
[email protected]
Colombia-South America
 
ラベル(1)
0 件の賞賛
返信
4 返答(返信)

2,485件の閲覧回数
alex_spotw
Contributor III
Hi Diego:

Any updates?

REgards,

Alex
0 件の賞賛
返信

2,485件の閲覧回数
Diego
Contributor I
SMAC 4.1.exe
There are some examples.
 
Thanks
0 件の賞賛
返信

2,485件の閲覧回数
alex_spotw
Contributor III
Diego:

The SMAC has many functionality, but it has some issues with interrupt reentrancy. You have to be careful with it. I have explained some things in other threads in this forum. Please check them.

Suerte!

Alex
Ex-alumno Javeriano
0 件の賞賛
返信

2,485件の閲覧回数
Diego
Contributor I
 
Do i have to implementate all of the  SPI commands?. Manage the packets (information)?, Manage all the ieee 802.15.4 standard?
 
 
 
 
0 件の賞賛
返信