S1/S9 Code Disasembler

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S1/S9 Code Disasembler

2,907 Views
BobMac
Contributor I
Does anyone know of a nifty little s1/s9 code viewer with a disas. included? I've got some 'hc08 source code from years gone by and would like to easily view it.
Best regards, Bob
Labels (1)
0 Kudos
Reply
3 Replies

1,640 Views
BobMac
Contributor I
As Charley Brown would say, "Aargh!" why didn't I think of that.
 Thanks a lot guys. I appreciate your help.
 There is a special feeling one gets after proclaming to the world, "I am a doofus" :smileywink:.
Regards, Bob
0 Kudos
Reply

1,640 Views
peg
Senior Contributor IV
Hi Bob,
 
Well I would not call it nifty or easy, but if you already have Codewarrior, you can use decoder.exe in the prog directory of your CW installation.
 
Regards
Peg
 
0 Kudos
Reply

1,640 Views
joerg
Contributor II

Hello BobMac

A simple way is to download a free HC08 ICS from PE (www.pemicro.com) If you start the simulator and then load the s19 file the code and the mnemonics are shown in a window.

Saluti Joerg

0 Kudos
Reply