S08QE8 Background Debug Mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S08QE8 Background Debug Mode

2,351件の閲覧回数
DavidoBG
Contributor II
I try to program my MCU S08QE8 with cyclone pro but i have error message when i try to connect emulator to MCU
Loading Target ...
Windows NT detected.
CYCLONE PRO detected - Flash Version 8.09
Frequency change to ~0hz.
Frequency change to ~0hz.
CYCLONE PRO detected - Flash Version 8.09
Frequency change to ~0hz.
Frequency change to ~0hz.
Frequency change to ~0hz.
Frequency change to ~0hz.
Frequency change to ~0hz.
Frequency change to ~8032hz.

Error: Can not enter background mode.

I check my RESET (Pin 1 of MCU) and BKGD (pin 2 of MCU) signals
On Pin 1 i have 0.4V i thonk OK to do reset.
On pin 2, i have 0.7V!!!
In fact i directly connect PIN 1 of BDM connector from Cyclone to Pin 2 of MCU. Is it correct?
I used an external power to supply MCU but i connect GND of MCU to Pin 2 of BDM connector
 
Somebody ou somewhere can i find some descriptions, explanation about connections between cyclone emulator and MCU S08QE8?
 
thanks
 
David
ラベル(1)
2 返答(返信)

1,517件の閲覧回数
alexod
Contributor I
I used an external power to supply MCU but i connect GND of MCU to Pin 2 of BDM connector

It might just be the way you phrased it but, you do have your external power supply's ground connected as well don't you?

0 件の賞賛
返信

1,517件の閲覧回数
celsoken
Contributor V
Dear Davido,

BDM physical interface is quite simple, it uses mainly BKGD.
In order to enter BKGD mode you have to have BKGD in 0V and reset the uC.
The problem is that sometimes reset pin is not programmed as that.
The only way to assure this is thru pwr-up reset.

Suggestion from someone who has burned more than 8 EVB BDMs: use 0.1A PPTCs in series with GND(2), BKGD(1), RST(4) and VDD(6 - if you use it). Pullups to VDD  from RST and BKGD are nice too.

Cheers,

Celso