S08QE32 load capacitors

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S08QE32 load capacitors

1,727件の閲覧回数
mlun
Contributor I

I'm about to try the QE32 with external 32kHz crystal RANGE=HGO=0.

The datasheet says that the load capacitors and series resistor are incorporated, but I can't find any recommendations for the crystals load capacitance.

Common 32kHz crystals have load capacitance 6-12pF.

Which load capacitance is best?

 

Magnus

ラベル(1)
0 件の賞賛
返信
1 返信

1,050件の閲覧回数
peg
Senior Contributor IV

Hello and welcome to the fora mlun,

 

As an example the DEMOQE board's schematic shows 22pF caps on xtal.

On my board there are no caps fitted, No Rf and Rs is zero ohms.

The manual does say in several places that this is correct for low range/low power mode.

Have not actually run external oscillator myself.

 

0 件の賞賛
返信