Vicente Gomez Salazar Hello,
Thank you for your promoted answer, I have followed you're suggesting but somehow when I tried to flash an off-board target using S08PT60-EVK, the S08PT60-EVK MC9S08JM60 got broken since I got the following Error also for the off-board target (S08PL4) but also for the onboard S08PT60 has stopped working:
fl::target -lc "Test1.0"
fl::target -b 0x40 0x200
fl::target -v off -l off
cmdwin::fl::device -d "MC9S08PL4_FLASH" -o "2kx16x1" -a 0xf000 0xffff
cmdwin::fl::image -f "C:\\NXP\\S08PT60-EVK\\Test.abs.s19" -t "Auto Detect" -re on -r 0xf000 0xffff -oe off
cmdwin::fl::erase image
Beginning Operation ...
-------------------------
Auto-detection is successful.
File is of type Motorola S-Record Format.
Performing target initialization ...
Error: Connect Failed.
Can't connect. The Debugger can not connect to the P&E device(HC/RS/S12Z GDI Protocol Adapter)
Error: Connect Failed.
Could you please advise if there is any way to reflash/reprogramme the MC9S08JM60 (programmer/debugger) of the S08PT60-EVK, in order to fix the kit?
Thanks in advance, Kind regards,
Shai