S08PT60-EVK RGB program

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S08PT60-EVK RGB program

2,062 Views
transistor_vaglienty
Contributor I

I need the original program that was include into the board,

1 Reply

2,027 Views
Pablo_Ramos
NXP Employee
NXP Employee

Hi @transistor_vaglienty,

The only software currently available for the S08PT60 is the example code provided in CodeWarrior v11.1 and the AN4690SW, which is available in the documentation section of the S08PT.

S08PT|8-bit 5V Full-featured MCU with EEPROM and TSI | NXP Semiconductors

Best Regards,
Pablo

0 Kudos
Reply