S08MP16 HSCMP to FTM2 synchronisation help required

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S08MP16 HSCMP to FTM2 synchronisation help required

1,206 Views
abicash
Contributor III

Hello

 

I am pretty amazed by the power of this 8-bit device and now i am replacing most of my SH8's and QG8's  with a MP16.

 

I need a few pointers or any help from learned members (in form of a snippet is most appreciated)

 

I have a MOSFET H-Bridge which i drive in 2 modes.

Mode-1 : Inverter mode in which all 4 MOSFETs generate a PWM Sine Wave

Mode-2 : Charge mode , in which the bottom FETs are switching to make a Boost converter. The PWM for these FETs is synced to Mains.

 

Mode-1 is complete now i have to get Mode-2 up and running.

I am planning to use a HSCMPx input to trigger the FTM2 (which is generating these PWM waveforms).

Please guide me how to get this done

 

Thanks and regards

Labels (1)
0 Kudos
Reply
1 Reply

1,119 Views
weapon
Senior Contributor I

Hi Jagtab,

Have you ever tried to use Processor Expert?  it can generate lots of examples as reference.

B.R

Weiping

0 Kudos
Reply