S08MP16 HSCMP to FTM2 synchronisation help required

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S08MP16 HSCMP to FTM2 synchronisation help required

1,153件の閲覧回数
abicash
Contributor III

Hello

 

I am pretty amazed by the power of this 8-bit device and now i am replacing most of my SH8's and QG8's  with a MP16.

 

I need a few pointers or any help from learned members (in form of a snippet is most appreciated)

 

I have a MOSFET H-Bridge which i drive in 2 modes.

Mode-1 : Inverter mode in which all 4 MOSFETs generate a PWM Sine Wave

Mode-2 : Charge mode , in which the bottom FETs are switching to make a Boost converter. The PWM for these FETs is synced to Mains.

 

Mode-1 is complete now i have to get Mode-2 up and running.

I am planning to use a HSCMPx input to trigger the FTM2 (which is generating these PWM waveforms).

Please guide me how to get this done

 

Thanks and regards

ラベル(1)
0 件の賞賛
返信
1 返信

1,066件の閲覧回数
weapon
Senior Contributor I

Hi Jagtab,

Have you ever tried to use Processor Expert?  it can generate lots of examples as reference.

B.R

Weiping

0 件の賞賛
返信