S08DZ60 A/D fluctuating

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S08DZ60 A/D fluctuating

ソリューションへジャンプ
4,491件の閲覧回数
jiaqihe
Contributor II

   I am using the S08DZ60 for graduation design, but I have a problem. The A/D sample value is always fluctuating,  the amplitude is about 10, and the voltage of the oscilloscope observation sampling point is stable. I tried all the methods I could think of, but it didn't work. I hope I can get any help, thank you very much. I will be very grateful if someone can help me. I really have no idea.

タグ(1)
0 件の賞賛
返信
1 解決策
4,329件の閲覧回数
jiaqihe
Contributor II

Thank you a lot. The problem is solved, my 5V reference voltage design is problematic, causing interference to A/D sampling. Redesigned and solved.

元の投稿で解決策を見る

0 件の賞賛
返信
9 返答(返信)
4,330件の閲覧回数
tonyp
Senior Contributor II

You could average multiple readings (say, 4) per sample to minimize the fluctuation.

And use the lowest clock for the A/D.

0 件の賞賛
返信
4,330件の閲覧回数
jiaqihe
Contributor II

I have averaged multiple readings, but it works not well. Then I change the A/D clock to 1MHz, but it doesn't work. Is the problem probably in the program?

0 件の賞賛
返信
4,330件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

I just read you have an error of 10 of 4096 (12 bit) ? 

Can you check if you have other modules enable at the same time that you are making the measurements? or if you have noise on the system, maybe you have a signal input in other pin that is affecting your ADC measurement 

Regards

0 件の賞賛
返信
4,330件の閲覧回数
jiaqihe
Contributor II

Thank you a lot. The problem is solved, my 5V reference voltage design is problematic, causing interference to A/D sampling. Redesigned and solved.

0 件の賞賛
返信
4,330件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

Excellent that you found the problem, let me know if you have more questions

0 件の賞賛
返信
4,330件の閲覧回数
tonyp
Senior Contributor II

Is that 10 out of 1023 (10 bit mode)?

0 件の賞賛
返信
4,330件の閲覧回数
jiaqihe
Contributor II

12 bit mode, and A/D sampling reference voltage is also stable. I have changed another MCU, but it didn't work.

0 件の賞賛
返信
4,330件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

Hi

Are you using high-speed mode?

We recommend to use low power configuration (ADLPC).

Regards

0 件の賞賛
返信
4,330件の閲覧回数
jiaqihe
Contributor II

I confirmed that I am using low power mode. And it didn't work.

0 件の賞賛
返信