S08 USB MSD bootloader - for JM32

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S08 USB MSD bootloader - for JM32

2,415 次查看
leesp
Contributor I

Has anyone tried the MC9S08 USB Mass Storage Device bootloader?

I know from AN3927, it works for MC9S08JM60. But does it work on MC9S08JM32, which has much smaller flash and RAM?

标签 (1)
0 项奖励
回复
3 回复数

2,017 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

i don;t have JM32 version an3927

Another option is using the Bootloader for the JM60 GUI, who is explained on application note AN3561, which can be found on the following link:

http://www.freescale.com/files/microcontrollers/doc/app_note/AN3561.pdf

I am attaching to this email; a CodeWarrior 6.3 project based on this application note, but migrated to MC9S08JM32 device.

0 项奖励
回复

2,017 次查看
leesp
Contributor I

Hi,

I know AN3561 is another option, but it needs Windows drivers.

I am using Windows 8, and I understand that the driver for Win8 does not exist (Freescale does not support this driver for Win8).

So my only option is AN3927. Did anybody try it on JM32?

0 项奖励
回复

2,017 次查看
3times1day
Contributor I

Hi,

Do you finish your AN3927+ MC9S08JM32 project?

I did AN3927+ MC9S08JM60. USB MSD bootloader works on Win 7 and Win 8.0, but it doesn't work on Win 8.1. Do you have same problem?

0 项奖励
回复