S08 SCI LBKD Interrupt

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S08 SCI LBKD Interrupt

1,312 Views
qiongyu
Contributor I

I'm using S12 communicate with S08 via SCI。When S08 enable the break detect interrupt(set SCIxS2.LBKDE),no ISR reply. See the wave on RX pin with 13clk low, and in debug mode, the SCIxS2.LBKDIF is set. But can not jmp to the ISR.

 

When S08 disable the break detect inerrupt(clr SCIxS2.LBKDE),the S08 will jmp to ISR with receiver buffer full and Framing Error. I think the baud rate is the same as S12.

Labels (1)
0 Kudos
Reply
1 Reply

1,151 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Hi, can you please tell me the device that you are using  (S08)

Thanks

Regards

Vicente Gomez

0 Kudos
Reply