Rx buffer on ZED

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Rx buffer on ZED

2,386件の閲覧回数
trailrr
Contributor I
Hi all
 
I has just started to work with zigbee technology. I am new to this technology. 
I am using the freescale Beekit beestack codebase 1.0.2. I am currently working on  a zigbee project and i am using 1 NCB and 1 SRB boards to test out the tx and rx between the ZED and ZC. I will like to find out whether is that any rx buffer at the ZED side (if there is, might i know where location of the buffer in the ZED firmware) and how the received data was being interpreted. Thanks
 
Regards,
 
Trailrr
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,484件の閲覧回数
Mads
Contributor V
Hi Trailrr,
 
first of all, you are not using the latest Beestack codebase. the latest version is 1.0.3.
Please go download the latest beekit on www.freescale.com/zigbee
 
To answer your question. there is not a single buffer that "just" contains the data that is received by the ZED.
 
The data recieved in an ZigBee is recieved in function called BeeAppDataIndication() in Beeapp.c as a pointer to a message.
 
I would recommend that you read the ZigBee application user's guide in order to learn how to use the demo application that comes with Beestack, and read and follow the instructions in The Beestack Application Developer's users guide in order to learn how to develop a ZigBee application.
 
BR,
Mads
 
 
0 件の賞賛
返信

1,484件の閲覧回数
trailrr
Contributor I
Hi Mads
 
Thanks for the reply. I will read up about it. In addition, I will like to know whether is there anyway I can do to the ZC code to allow ZED to bind to the ZC when the ZC is in application mode? As I need my ZC to stay in application mode and at the same time allow other ZEDs to bind to the ZC. Thank you.
 
Regards,
 
trailrr
0 件の賞賛
返信