Relative values of A2D Input Leakage Currents

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Relative values of A2D Input Leakage Currents

861 Views
stephenwhite
Contributor I

The S9S08RNA16W2MLCR A2D data sheet specifies the range of input pin leakage currents as  -1uA to +1uA.  I have high impedance series input resistors (500Kohm to 1MHom) to a pair of analog signals the connect to two microcontroller A2D input pins.   Can I assume that the leakage currents of the two A2D input pins will match if the input voltage are the same?  That is, if one pin leaks 1uA , will the other pin leak 1uA as well if both input voltage are the same?

Labels (1)
Tags (1)
0 Kudos
Reply
0 Replies