Relative values of A2D Input Leakage Currents

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Relative values of A2D Input Leakage Currents

877 次查看
stephenwhite
Contributor I

The S9S08RNA16W2MLCR A2D data sheet specifies the range of input pin leakage currents as  -1uA to +1uA.  I have high impedance series input resistors (500Kohm to 1MHom) to a pair of analog signals the connect to two microcontroller A2D input pins.   Can I assume that the leakage currents of the two A2D input pins will match if the input voltage are the same?  That is, if one pin leaks 1uA , will the other pin leak 1uA as well if both input voltage are the same?

标签 (1)
标记 (1)
0 项奖励
回复
0 回复数