Hello There,
While configuring the timer channel 0 of MC68HC908QY4 Microcontroller, i am getting a strange problem of not been able to set the TSC0_ELS0A and TSC0_ELS0B bits to enable "Capture on rising or falling edge" mode. I am using cyclone pro debugger and while stepping on the respective instructions, the cyclone pro throws an error "Error: Unable to go into background mode".
Even if i set the breakpoint after the instructions, it never reaches the breakpoint and hangs. I have tried setting the ELS0A & ELS0B bits by bit-wise addressing mode and also by addressing TSC0 register. Both ways i am encountering the same problem. While addressing the other bits of TSC0 register, i do not get any error.
Kindly suggest if the input capture functionality in the code below is imlemented in a correct way.
The code is as follows. Please see the function Input_Capture_Init (). The error JPEG file is also attached.
/*************************************** Code ******************************************/
#include <hidef.h> /* for EnableInterrupts macro */
#include "derivative.h" /* include peripheral declarations */
#define COP_ENABLE 0 // Enable Watchdog
#define STOP_INSTRUCTION_DISABLE 0 // Disable Stop instruction
#define STOP_RECOVERY_LONG 0 // Stop Mode Recovery after 4096 cycles
#define LVI_3V 0 // 3V operating voltage of LVI module
#define LVIPWR_ENABLE 0 // Enable LVI Module Power
#define LVIRST_ENABLE 0 // Enable LVI Module Reset
#define LVISTOP_DISABLE 0 // Disable LVI during STOP-Mode
#define COP_LONG_RESETTIME 0 // Watchdog resets after 262128* BUSCLK*4
#define RSTEN_ACTIVE 0x01 // Reset function active in pin
#define INTERNAL_OSC 0 // Internal oscillator
#define IRQ_ACTIVE 0x40 // Interrupt request function active
#define IRQ_PULLUP_CONNECT 0 // IRQ pin pullup connected between IRQ pin and VDD
/* Input capture */
#define CAPTUR_ON_RISING_EDG 0x04
#define CAPTUR_ON_FALLING_EDG 0x08
#define CAPTUR_ON_RISING_OR_FALLING_EDG 0x0C
/* Configuration settings for MSxA - Mode Select Bit A */
#define ENBL_INPUT_CAPTR 0x00
#define ENBL_UNBUFRD_PWM 0x10
#define ENBL_UNBUFRD_OUTPUT_CMPR 0x10
typedef unsigned short uint16;
typedef unsigned char uint8;
void Set_PWM_out_Param (void);
void SystemInit(void);
void PWM_out_Init (void);
void MCU_init(void); /* Device initialization function declaration */
void delay (void);
void Input_Capture_Init (void);
void Read_Freq (void);
uint16 Read_TIM_Cntr (void);
void main(void)
{
/* include your code here */
SystemInit();
PWM_out_Init();
Input_Capture_Init();
Set_PWM_out_Param();
for(;![]()
{
}
}
void SystemInit(void)
{
char *Trim_Val;
Trim_Val = (char*)0xFFC0;
OSCTRIM = *Trim_Val;
// Write CONFIG1-Register (Write-Once-Register)
CONFIG1 = ( COP_ENABLE | // Enable Watchdog
STOP_INSTRUCTION_DISABLE | // Disable Stop instruction
STOP_RECOVERY_LONG | // Stop Mode Recovery after 4096 cycles
LVI_3V | // 5V operating voltage of LVI module
LVIPWR_ENABLE | // Enable LVI Module Power
LVIRST_ENABLE | // Enable LVI Module Reset
LVISTOP_DISABLE | // Disable LVI during STOP-Mode
COP_LONG_RESETTIME // Watchdog resets after 262128* BUSCLK*4
);
// Write CONFIG2-Register (Write-Once-Register)
CONFIG2 = ( RSTEN_ACTIVE | // Reset function active in pin
INTERNAL_OSC | // Inernal Crystal oscillator
IRQ_ACTIVE | // Interrupt request function active
IRQ_PULLUP_CONNECT // IRQ pin pullup connected between IRQ pin and VDD
);
}
void PWM_out_Init (void)
{
DDRA = 0x02; /* Configuring PTA1 pin as output */
PTA = 0x02; /* Driving high */
DDRB = 0x02;
PTB = 0x02;
}
void Set_PWM_out_Param (void)
{
/********** PWM signal Frequency Settings **********/
/* Loading the values in appropriate registers */
TMODH = 0;
TMODL = 39; /* Frequency 160 * (1/800 KHz) = 5KHz*/
TCH1L = 0;
TCH1L = 20; /* 50% Duty Cycle */
TSC1 = 0x16;
/* Setting the pre-scalar value as ÷ 4, i.e. 3.2MHz÷4 = 800KHz and starting the counter*/
TSC = 0x02;
}
void Input_Capture_Init (void)
{
TSC = 0x30; /* Stop and Reset the TIM counter */
/* Clear the TIM channel registers */
TCH0H = 0;
TCH0L = 0;
/* Enabling input capture at TCH0 channel with rising/falling edge capture */
/* The instruction below is causing the problem */
TSC0 = 0x0C;
//TSC0 = ENBL_INPUT_CAPTR | CAPTUR_ON_RISING_OR_FALLING_EDG;
}
/* Function to read the frequency of captured signal */
void Read_Freq (void)
{
uint16 Time_Stamp1;
uint16 Time_Stamp2;
uint16 Time_Stamp3;
float Time_Period;
uint16 TIM_Count;
uint16 Freq;
Time_Stamp1 = Read_TIM_Cntr();
Time_Stamp2 = Read_TIM_Cntr();
Time_Stamp3 = Read_TIM_Cntr();
/* Calculate the time */
TIM_Count = (Time_Stamp2 - Time_Stamp1) + (Time_Stamp3 - Time_Stamp2);
/* With pre-scalar value of ÷ 4, i.e. 3.2MHz÷4 = 800KHz, Time period = 1.25 uS */
Time_Period = (1/800000)* TIM_Count;
Freq = 1/Time_Period;
}
/* Function to capture the TIM counter value of the input capture function */
uint16 Read_TIM_Cntr (void)
{
uint8 Byte_TCH0H;
uint8 Byte_TCH0L;
uint16 Time_Stamp;
/* Wait till active edge occurs on the channel 0 pin */
while (TSC0_CH0F != 1);
/* Read the TIM channel 0 status and control register */
Byte_TCH0H = TCH0H;
Byte_TCH0L = TCH0L;
/* Clear the CH0F bit for next capture */
TSC0_CH0F = 0;
/* Store the counter value */
Time_Stamp = (Byte_TCH0H<<8) | Byte_TCH0L;
return (Time_Stamp);
}
Hello,
There are some basic problems with your approach.
// Global variables:volatile uint16 old_val, new_val;
uint16 period; while (!TSC0_CH0F); // Wait for input capture event TSC0_CH0F = 0; // Clear flag old_val = new_val; // Transfer previous capture value new_val = TCH0; // Current capture value period = new_val - old_val;
Regards,
Mac
Thanks Mac. I am polling the port pin instead of input capture and it is working fine now.