Re: an2295sw

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,735件の閲覧回数
RA
Contributor I

Hello everybody:

Does anybody know if there will be a C version for this AP note?

Thanks so much

ラベル(1)
0 件の賞賛
返信
1 解決策
1,459件の閲覧回数
lydia_ziegler
NXP Employee
NXP Employee

Hi Raef,

This code is all written in ASM and meant to be very low level and take advantage of all the different features of the various supported devices (on-chip bootloaders, etc).  I know of no plans to create a C version.

Best regards!

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,460件の閲覧回数
lydia_ziegler
NXP Employee
NXP Employee

Hi Raef,

This code is all written in ASM and meant to be very low level and take advantage of all the different features of the various supported devices (on-chip bootloaders, etc).  I know of no plans to create a C version.

Best regards!

0 件の賞賛
返信