Random reception of data packets out of reset - ZigBee

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Random reception of data packets out of reset - ZigBee

1,182件の閲覧回数
rs
Contributor I
Hello,
We have a setup where a coordinator transmits heartbeat data packets for every 1/16th of a second i.e, 64 ms. When a router comes out of reset receives the first heartbeat data packet so random that the time interval varies from 50 ms to more than 2 seconds.
I am using BeeStack Codebase for my project. I have verified at my application level code that BeeAppTask function which calls RxZigBee function when the device receives the data packet is not invoked by any other source.
I really have no idea from where the delay of receiving the data packets that were transmitted so regularly by coordinator is being inserted. I am supposed to receive the heartbeat data packet as soon as the router comes out of reset and then I make the router to stay awake as it keeps receiving the heart beat data packets.
 
I am in a deadlock situation where I can't proceed any further. Could you please help me out providing some tips to debug and figure out from where the delay is being inserted.
 
Thank you
 
 
Add ZigBee to the subject.


Message Edited by NLFSJ on 2007-11-28 06:22 AM
ラベル(1)
0 件の賞賛
返信
1 返信

595件の閲覧回数
Mads
Contributor V
Hi,
 
I have answered you question through the SR you also have created.
 
/Mads
0 件の賞賛
返信