RTC timer Initialization ..

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RTC timer Initialization ..

5,942 Views
UPP
Contributor I

 hi  i am used mc9so8dz60 demo board .. i initialize RTC  timer .. but it is not working so please help me to int RTC timer..here is my code 

void timerint(void);

void main(void)

 {

EnableInterrupts;

timerint();

SOPT1=0x00;

SOPT2=0x00;
      for(; :smileywink: 

 { 

        PTFD_PTFD3=0; 

 PTFDD_PTFDD3=1; 

 Lcd16x2Init(); 

 Cpu_Delay100US(1000);   

 DispMsg(msg,16,0x080); 

 Cpu_Delay100US(1000); 

 }

  for(; :smileywink:

{ } /* loop forever */  /* please make sure that you never leave main */

}

 

 

 

 

void timerint(void)

{

RTCMOD=0;

RTCSC_RTCPS =15;

RTCSC_RTCLKS=0;

}

#pragma TRAP_PROCvoid RTC_ISR(void)

{  

RTCSC=RTCSC|0x80;  

PTCD_PTCD5=0;     // led on

 PTCDD_PTCDD5=1;  

Cpu_Delay100US(100);  

PTCD_PTCD5=1;  // led off

PTCDD_PTCDD5=1;

 Cpu_Delay100US(100);

}

Labels (1)
0 Kudos
Reply
11 Replies

5,469 Views
bigmac
Specialist III

Hello,

 

I see that your code does not set the RTIE bit within RTCSC.  To avoid this type of problem, it is better to simultaneously write all bits when initialising a control register, i.e.  RTCSC = 0x9F;

 

Some other comments about your code -

  1. You should not globally enable interrupts until after initialisation of all peripherals, including the RTC module, has been done.
  2. It is an extremely poor programming practice to incorporate significant delays within any ISR code.  The ISR code should exit as quickly as possible, so that the execution of any other ISRs will not be unnecessarily delayed.

Regards,

Mac

 

0 Kudos
Reply

5,469 Views
UPP
Contributor I

thanks for your reply ...

                                    but i still found the same problem i m no getting the RTC interrupt & i do changes that you suggest .. here is my code.. when i run the program..... program get hang & lcd doesnt show any thing...

but whn i remove  EnableInterrupts  then program run & lcd show the message but doesnt get the interrupt..

 

 

#include <hidef.h> /* for EnableInterrupts macro */

#include "derivative.h" /* include peripheral declarations */

#include "lcd16x2_4bit.h"

void timerint(void); 

void RTC_ISR(void) ;

byte msg[]={"SPRY LOGIC LTD.."};

word counter=0;

void main(void)

 {

SOPT1=0x00;

SOPT2=0x00;

timerint();

PTFD_PTFD3=0;

PTFDD_PTFDD3=1;

Lcd16x2Init();

EnableInterrupts;      

    for(;:smileywink: 

    { 

       Cpu_Delay100US(1000);

        DispMsg(msg,16,0x080);   

        Cpu_Delay100US(1000);

     }

     for(;:smileywink:

       {}

  }

void timerint(void)

{

RTCMOD=0X00;

RTCSC=0x9F;
}

#pragma TRAP_PROC

 void RTC_ISR(void)

 {      

RTCSC=RTCSC|0x80;  

PTCD_PTCD5^=1;  

PTCDD_PTCDD5=1;

}

0 Kudos
Reply

5,469 Views
bigmac
Specialist III

Hello,

 

If your Lcd16x2Init() function relies on the use of interrupts, you will need to shift its position.

 

Regards,

Mac

 

0 Kudos
Reply

5,469 Views
UPP
Contributor I

hi my lcd int() function is doenot reli on interrupt.... but i still got  the same problem

 

 

0 Kudos
Reply

5,469 Views
kef
Specialist I

Is RTC vector pointing to RTC_ISR()? Did you set up RTC vector?

0 Kudos
Reply

5,469 Views
UPP
Contributor I

hi ..  i think didnt ponit the vector ... but i dont how to point the vector can you please tell me how to point the vector of any interrupt using #pragma.. 

0 Kudos
Reply

5,469 Views
JimDon
Senior Contributor III

If you declare your function like this:

 interrupt  VectorNumber_Vrtc void   RTC_ISRr(void) {

 

It will go into the vector table. I like this method, as if you have reuseable code you can just add it to the project, and it goes into the vector table.

 

The other option is to find the vector table in your project and put it in.

 

 

0 Kudos
Reply

5,469 Views
UPP
Contributor I

hi thank you ... for reply ..

                                but  i have another problem regarding the port interrupt ... i use the PTA  As an interrupt  so i want to reconized the on which  pin of PTA  interrupt is coming .... so how to reconzie ...   

0 Kudos
Reply

5,469 Views
bigmac
Specialist III

Hello,

 

You will need to read the port input status from within the ISR, to determine the pin that caused the interrupt.  This implies that the active level must be present for a period that exceeds the interrupt latency period, which may also include the period of other ISRs that are already executing when the the input event occurs.

 

If more than one input pin is enabled, and if a previously detected pin remains in an active state, input transitions from the other pins will not be detected.  This applies even with the use of edge triggered mode for the interrupt,  The solution is to temporarily disable each pin whilst it remains in an active state.

 

For mechanical switch use, a debounce period will also need to be allowed.  An active pin would be temporarily disabled for a minimum period, usually within the range 10 to 100 milliseconds.

 

Regards,

Mac

 

0 Kudos
Reply

5,469 Views
JimDon
Senior Contributor III

Based on the tech ref and the block diagram, I don't think you can because the pins ar or'ed together to generate the interrupt and there does not seem to be a register holding the individual interupt states.

In other words, there is a single interrupt flip flop per port.

Also be aware that if you are using levels, you must make the level "go away" or you will keep getting interrupts if you leave that pin enabled for level interrupts. This effect will cause you code the seem crashed, as all it will be doing is servicing that interrupt.

 

Did the timer issue get resolved?

 

0 Kudos
Reply

5,469 Views
UPP
Contributor I

hello jim 

 

          Sorry for let but i am out of station for some day.. ya the timer isuue get resolved but i have aother issur regarding the how to use the temperature sensor in MC9S08DZ60.. i confuger sensor as oer data sheet but it didnt work properly.. so tel me hoe to use the temp sensor in application...    

0 Kudos
Reply