RS232 Serial Terminal

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RS232 Serial Terminal

7,294 Views
eagletek
Contributor I
Hello,
I am performing some tests with the 19132 SARD board and I am interfacing with the RS232 port of the board.

I would like to know if anyone can suggest me a freeware program to use
under windows xp as serial terminal.

I tried using hyper terminal but I got a problem after a period of usage.. i.e. it doesn't accept any input anymore.

bye
Marco
Labels (1)
0 Kudos
Reply
6 Replies

2,749 Views
killabyte
Contributor I
write to my personal email account then ill send back a easy program to work rs232 port.

[email protected]

best

killabyte
0 Kudos
Reply

2,749 Views
Encoder
Contributor I
Hyperterminal usually saves a log file somewhere.
Perhaps this log file is simply full. Try to delete the log file and restart the program: you need to re-configure it too.
0 Kudos
Reply

2,749 Views
new
Contributor I
Hello,
I am working with sard 13192, hcs08gt60, But I am not able to reprogram flash using RS232.  I dont have BDM so I can reprogram it using the RS232 only. Which tool is required to reprogram through RS232? how is the procedure for this.
Please help to reprogram it.
 
Navin
0 Kudos
Reply

2,749 Views
peg
Senior Contributor IV

Hi Marco,

Quote:

"I tried using hyper terminal but I got a problem"

What! you only found one problem!!!:smileyvery-happy:

 

Try this:

http://realterm.sourceforge.net/

and I guarantee you will never try use hyperterminal again!

Peg

0 Kudos
Reply

2,749 Views
irob
Contributor V

peg wrote:

Try this: http://realterm.sourceforge.net/ and I guarantee you will never try use hyperterminal again!



I should have checked here first for serial port terminal programs. After much searching for open source alternatives, I found RealTerm too. And yep, Peg's right. It's wonderful!
0 Kudos
Reply

2,749 Views
peg
Senior Contributor IV
Hi rob,
 
See here for the very latest versions:
 
 
0 Kudos
Reply