RS08LA8 use of ICSIRCLK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RS08LA8 use of ICSIRCLK

ソリューションへジャンプ
1,322件の閲覧回数
gosa
Contributor I

Hi

I'm new in freescale microcontrollers and I start with RS08LA. I check and test what clocksource I have for system, timer, etc and I woundering that I can not found supported ICSIRCLK from internal clock source (ICS) for system clock distribution (figure 1-2 in datasheet). So what is the use of ICSIRCLK?

 

KR

ラベル(1)
0 件の賞賛
返信
1 解決策
1,220件の閲覧回数
bigmac
Specialist III

Hello KR,

The ICS module is present in many MCU derivatives, from both S08 and RS08 families.  I guess the answer to your query is that the ICSIRCLK signal is present within the module itself, but is never used for the RS08 device that you are using.  It would seem an unfortunate omission if this is not clarified in the introductory paragraphs of the ICS chapter within the specific datasheet.

Regards,

Mac

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,220件の閲覧回数
Monica
Senior Contributor III

Hello KR

I found this paragraph in the Data Sheet that might reply to your question:

10.4.5 Internal Reference Clock

When IRCLKEN is set the internal reference clock signal will be presented as ICSIRCLK, which can be used as an additional clock source. The ICSIRCLK frequency can be re-targeted by trimming the period of the internal reference lock. This can be done by writing a new value to the TRIM bits in the ICSTRM register. Writing a larger value will slow down the ICSIRCLK frequency, and writing a smaller value to the ICSTRM register will speed up the ICSIRCLK frequency. The TRIM bits will effect the ICSOUT frequency if the ICS is in FLL engaged internal (FEI), FLL bypassed internal (FBI), or FLL bypassed internal low power (FBILP) mode. The TRIM and FTRIM value will not be affected by a reset.

Let me know if it does address your question, I will be around!

Regards.

0 件の賞賛
返信
1,220件の閲覧回数
gosa
Contributor I

Hi Monica

Your link of data sheet reference to S08SH8 but I use the RS08LA8. In the RS08LA8 I can not found any usage of ICSIRCLK. It will be distributed in the Internal Clock Source ICS (figure 9-2) but does not appear in the clock connection diagramm (figure 1-2). I just wondering about that issue.

Regards

0 件の賞賛
返信
1,221件の閲覧回数
bigmac
Specialist III

Hello KR,

The ICS module is present in many MCU derivatives, from both S08 and RS08 families.  I guess the answer to your query is that the ICSIRCLK signal is present within the module itself, but is never used for the RS08 device that you are using.  It would seem an unfortunate omission if this is not clarified in the introductory paragraphs of the ICS chapter within the specific datasheet.

Regards,

Mac

0 件の賞賛
返信