RS08KA2 two hour delay timer

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RS08KA2 two hour delay timer

2,428 Views
Rodo55
Contributor I

I'm a novice and I'm looking for help on a two hour delay timer for a project I'm working on.

I'm using a RS08KA2 MC and it doesn't have a RTC so I've nested loops to create a long delay but it isn't very accurate. Does anyone know how to implement a long delay in the KA2 that may be easier to implement and more accurate? I've looked at AN3413 Low Cost digital timer but it ties in a ADC and I can't seem to understand the code.

 

Below is what I've done to get a long delay and it works but seems like a very bad way to do it.

I included all the code since it's such a small program.

 

Any advice would be appreciated,

 

Thanks,

Rod

 


  ORG RAMStart
counter:        DS.B  1
counter2:      DS.B  1          
counter3:      DS.B  1
time2:          DS.B  1

; Const Section
ConstSection:  SECTION
time:           DC.B  $FF
 
; Code Section

            ORG ROMStart
   
;*******************************************************************************************
; Peripheral Initialization
;*******************************************************************************************
init:

;CONFIGURES SYSTEM CONTROL
    mov #HIGH_6_13(SOPT), PAGESEL 
    mov #$03, MAP_ADDR_6(SOPT)      ; Disables COP, enables BKGD (PTA3) and RESET (PTA2)                                 

;CONFIGURES CLOCK (FEI Operation Mode)        
    mov #HIGH_6_13(NV_ICSTRM),PAGESEL 
    lda MAP_ADDR_6(NV_ICSTRM)        
   sta ICSTRM                      ; Sets trimming value  
   clr ICSC1                         ; Selects FLL as clock source and disables it in stop mode
   clr ICSC2                         ; ICSOUT = DCO output frequency  
wait_clock:
    brset CLKST,ICSSC,wait_clock      ; Waits until FLL is engaged
   
;CONFIGURES TIMER
    mov #$70, MTIMSC                    ; Enables interrupt, stops and resets timer counter
    mov #$FF, MTIMMOD                 ; MTIM modulo = 256 counts before interrupt
    mov #$08, MTIMCLK                  ; Selects fBUS as reference clock (8 MHz)


;CONFIGURES I/O CONTROL PORT    
    mov #$31, PTADD                   ; Configures PTA0, PTA4 and PTA5 as output,PTA1 as an Input
    mov #HIGH_6_13(PTAPE), PAGESEL 
    mov #$04, MAP_ADDR_6(PTAPE)       ; Enables Pull UP on PTA2  

;CONFIGURES KEYBOARD INTERRUPTS (KBI)
    mov #$00, KBIES                   ; Selects Falling Edge/Low on Pin
    mov #$02, KBIPE                   ; PTA1 as KBI input
    mov #$06, KBISC                   ; Clears any false interrupts
   
   
    clr PTAD                          ; Clears PTA port
    rts

 

 

;*******************************************************************************************
; Entry Point
;*******************************************************************************************
_Startup:
main:
    bsr init
    clr counter
    clr counter2
    clr counter3

main_loop:

loopRelay:
   
    mov #HIGH_6_13(SIP1),PAGESEL        
    brset 4,MAP_ADDR_6(SIP1),RelayOn      ;If button pushed goto Relay on
   
    bra loopRelay
                                                ;No push button continue to wait
RelayOn:
    bset 2, KBISC                         ;Clear KBI Interrupt
    bset 5, PTAD                          ;Turn on Relay LED
    bset 4,PTAD                           ;Turn on Relay

 

;BELOW IS THE NESTED DELAY LOOPS I USED  

 

StartDelay:
    mov #$60,MTIMSC

    bclr 4,MTIMSC                         ; Start MTIM counter

    wait
    lda counter
    cbeqa #255,Delay2
    inc counter
    bra StartDelay

Delay2:
    clr counter
    lda counter2
    cbeqa #55,Delay3
    inc counter2
    bra StartDelay
   
Delay3:
    clr counter
    clr counter2
    lda counter3
    cbeqa #57, RelayOff
    inc counter3
    bra StartDelay

 

RelayOff
    clr counter
    clr counter2
    clr counter3
    bclr 5,PTAD
    bclr 4,PTAD
    bra loopRelay

Labels (1)
0 Kudos
Reply
2 Replies

1,530 Views
bigmac
Specialist III

Hello Rod,

 

Using the MTIM for such a long time delay, I might suggest -

  1. Use XCLK (16kHz) as the MTIM source, rather than the bus clock.
  2. Set the prescale value to maximum (256), to increase the overflow period as much as possible.

With these settings, the MTIM clock frequency should be 62.5 Hz, assuming the reference clock is properly trimmed. Now for a free-running MTIM, the overflow period should be 4.096 seconds. However, if the MTIMMOD value were to be set to decimal 249, the overflow period should be exactly 4.0 seconds, which may be more convenient to work with.

 

A two-hour timeout period now requires that decimal 1800 overflows should occur, and this requires a 16-bit counter. Consider the following untested code snippet:

 

DELAY EQU   1800

count DS.W  1

...


StartDelay:

     mov   #(DELAY/256),count   ; High byte

     mov   #(DELAY%256),count+1 ; Low byte

     mov   #$60,MTIMSC          ; Start MTIM counter

     mov   #HIGH_6_13(SIP1),PAGESEL

loop1:

     wait

     brclr 2,MAP_ADDR_6(SIP1),loop1 ; Wait for MTIM overflow

 

     mov   #HIGH_6_13(MTIMSC),PAGESEL

     bclr  7,MAP_ADDR_6(MTIMSC)     ; Clear flag 

 

     lda count+1 ; Decrement word value

     bne next1

     dec count

next1:

     dec count+1

     lda count   ; Test for timeout

     ora count+1

     bne loop1   ; Loop if not timeout

 

     ; Do timeout action here

 

 

Regards,

Mac

Message Edited by bigmac on 2009-09-09 02:58 PM
0 Kudos
Reply

1,530 Views
Rodo55
Contributor I

Thanks Mac,

 

I'll give that a try.

 

Have a great day,

 

Rod

0 Kudos
Reply