RS08, When ICS uses a wrong RDIV value, MCU works the same as with a right value.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RS08, When ICS uses a wrong RDIV value, MCU works the same as with a right value.

ソリューションへジャンプ
2,326件の閲覧回数
w_tension
Contributor III

Using extern 5MHz clock, set bus to 10MHz, When I use RDIV other than divide 128, MCU work the same.

Strange, is it?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,089件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

Normally the device after reset set the ICS to use the internal clock, (FEI), so probably your device is running with the internal clock, you can check it debuging the ICS register using code warrior.

regards

Vicente Gomez

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,089件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

Hi

Are you sure that the MCU is running with the external clock?

0 件の賞賛
返信
2,089件の閲覧回数
w_tension
Contributor III

Not quite sure. Just find serial communication still working.

UM doesn't mention what happens when a abnormal value is used.

0 件の賞賛
返信
2,090件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

Normally the device after reset set the ICS to use the internal clock, (FEI), so probably your device is running with the internal clock, you can check it debuging the ICS register using code warrior.

regards

Vicente Gomez

0 件の賞賛
返信