RS08, When ICS uses a wrong RDIV value, MCU works the same as with a right value.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

RS08, When ICS uses a wrong RDIV value, MCU works the same as with a right value.

跳至解决方案
2,362 次查看
w_tension
Contributor III

Using extern 5MHz clock, set bus to 10MHz, When I use RDIV other than divide 128, MCU work the same.

Strange, is it?

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
2,125 次查看
vicentegomez
NXP TechSupport
NXP TechSupport

Normally the device after reset set the ICS to use the internal clock, (FEI), so probably your device is running with the internal clock, you can check it debuging the ICS register using code warrior.

regards

Vicente Gomez

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,125 次查看
vicentegomez
NXP TechSupport
NXP TechSupport

Hi

Are you sure that the MCU is running with the external clock?

0 项奖励
回复
2,125 次查看
w_tension
Contributor III

Not quite sure. Just find serial communication still working.

UM doesn't mention what happens when a abnormal value is used.

0 项奖励
回复
2,126 次查看
vicentegomez
NXP TechSupport
NXP TechSupport

Normally the device after reset set the ICS to use the internal clock, (FEI), so probably your device is running with the internal clock, you can check it debuging the ICS register using code warrior.

regards

Vicente Gomez

0 项奖励
回复