RS08, When ICS uses a wrong RDIV value, MCU works the same as with a right value.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RS08, When ICS uses a wrong RDIV value, MCU works the same as with a right value.

Jump to solution
2,254 Views
w_tension
Contributor III

Using extern 5MHz clock, set bus to 10MHz, When I use RDIV other than divide 128, MCU work the same.

Strange, is it?

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
2,017 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Normally the device after reset set the ICS to use the internal clock, (FEI), so probably your device is running with the internal clock, you can check it debuging the ICS register using code warrior.

regards

Vicente Gomez

View solution in original post

0 Kudos
Reply
3 Replies
2,017 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Hi

Are you sure that the MCU is running with the external clock?

0 Kudos
Reply
2,017 Views
w_tension
Contributor III

Not quite sure. Just find serial communication still working.

UM doesn't mention what happens when a abnormal value is used.

0 Kudos
Reply
2,018 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Normally the device after reset set the ICS to use the internal clock, (FEI), so probably your device is running with the internal clock, you can check it debuging the ICS register using code warrior.

regards

Vicente Gomez

0 Kudos
Reply