RAM values changes unexpectedly

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RAM values changes unexpectedly

ソリューションへジャンプ
2,999件の閲覧回数
Jonathanp
Contributor I

Hi,

 

First of all excuse my low english level.  Something extrange happend to me....When I run the follow code (I'm using an AP16)

 

void CONVERT_DATA(void)
{
  TEMPORAL1=MSGRECEIVED[17];
  TEMPORAL1=TEMPORAL1-48;
  LATITUDE=TEMPORAL1*10;
  TEMPORAL1=MSGRECEIVED[18];
  TEMPORAL1=TEMPORAL1-48;
  LATITUDE=LATITUDE+TEMPORAL1;
 
  TEMPORAL1=MSGRECEIVED[19];
  TEMPORAL1=TEMPORAL1-48;
  MIN=TEMPORAL1*100000;
  TEMPORAL1=MSGRECEIVED[20];
  TEMPORAL1=TEMPORAL1-48;
  MIN=MIN+TEMPORAL1*10000;
 
 
  TEMPORAL1=MSGRECEIVED[22];
  TEMPORAL1=TEMPORAL1-48;
  MIN=MIN+TEMPORAL1*1000;
  TEMPORAL1=MSGRECEIVED[23];
  TEMPORAL1=TEMPORAL1-48;
  MIN=MIN+TEMPORAL1*100;
  TEMPORAL1=MSGRECEIVED[24];
  TEMPORAL1=TEMPORAL1-48;
  MIN=MIN+TEMPORAL1*10;
  TEMPORAL1=MSGRECEIVED[25];
  TEMPORAL1=TEMPORAL1-48;
  MIN=MIN+TEMPORAL1;
 
  MIN=MIN/600000;
  LATITUDE=LATITUDE+MIN;  
 
  TEMPORAL1=MSGRECEIVED[29];
  TEMPORAL1=TEMPORAL1-48;
  LONGITUDE=TEMPORAL1*100;
  TEMPORAL1=MSGRECEIVED[30];
  TEMPORAL1=TEMPORAL1-48;
  LONGITUDE=LONGITUDE+TEMPORAL1*10;
  TEMPORAL1=MSGRECEIVED[31];
  TEMPORAL1=TEMPORAL1-48;
  LONGITUDE=LONGITUDE+TEMPORAL1;
 
  TEMPORAL1=MSGRECEIVED[32];
  TEMPORAL1=TEMPORAL1-48;
  MIN=TEMPORAL1*100000;
  TEMPORAL1=MSGRECEIVED[33];
  TEMPORAL1=TEMPORAL1-48;
  MIN=MIN+TEMPORAL1*10000;
 
 
  TEMPORAL1=MSGRECEIVED[35];
  TEMPORAL1=TEMPORAL1-48;
  MIN=MIN+TEMPORAL1*1000;
  TEMPORAL1=MSGRECEIVED[36];
  TEMPORAL1=TEMPORAL1-48;
  MIN=MIN+TEMPORAL1*100;
  TEMPORAL1=MSGRECEIVED[37];
  TEMPORAL1=TEMPORAL1-48;
  MIN=MIN+TEMPORAL1*10;
  TEMPORAL1=MSGRECEIVED[38];
  TEMPORAL1=TEMPORAL1-48;
  MIN=MIN+TEMPORAL1;
 
  MIN=MIN/600000;
  LONGITUDE=LONGITUDE+MIN;  
 
 
  TEMPORAL1=MSGRECEIVED[44];
  TEMPORAL1=TEMPORAL1-48;
  SATELITES=TEMPORAL1*10;
  TEMPORAL1=MSGRECEIVED[45];
  TEMPORAL1=TEMPORAL1-48;
  SATELITES=SATELITES+TEMPORAL1;                 
}

 

The values of MSGRECEIVED changes and I don't understand why it happen if I don't assing this array in this funtion I only read it. If you can help me I'll really apreciate it. 

 

Regards,

Jonathan

Message Edited by Jonathanp on 2009-04-16 04:44 AM
ラベル(1)
0 件の賞賛
返信
1 解決策
2,081件の閲覧回数
Lundin
Senior Contributor IV
Variables changing unexpectedly is almost always caused by stack overflow. Try to make the stack larger and see if this solves the problem.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,082件の閲覧回数
Lundin
Senior Contributor IV
Variables changing unexpectedly is almost always caused by stack overflow. Try to make the stack larger and see if this solves the problem.

0 件の賞賛
返信
2,081件の閲覧回数
Jonathanp
Contributor I

Thankyou Lundin I made the stack larger and it solved the problem.

 

Jonathan

0 件の賞賛
返信