Question on MMA7660 availability

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Question on MMA7660 availability

ソリューションへジャンプ
2,099件の閲覧回数
Bobli
Contributor I

Hi,

 

In Digikey search “accelerometer”, and sort the results by price from low to high (registered user), MMA7660 turns out to be the No.1 cheap product among its total 661 accelerometers’ stock, costing

 

MMA7660FCT             $1.21

MMA7660FCR1           $0.67

 

for each unit.

 

I have two questions on MMA7660:

 

  1. I have heard from a vendor that MMA7660 is already obsolete. However, I downloaded MMA7660FC Manual and its date of release is Nov.2009, which is less than two years from now. Is it really obsolete, or is still active? When will Freescale discontinue it?
  2. The two products listed above have different prices, with the first almost twice of the second, and the only difference name is between suffix “T”  and “R1”. What does these suffixes mean? What are the differences between the two products?

 

 

 

Bob

ラベル(1)
0 件の賞賛
返信
1 解決策
1,897件の閲覧回数
bigmac
Specialist III

Hello Bob,

 

According to the Freescale website, this part has the classification of "maturity/saturation" which means that it is still active.

The T suffix refers to "tray" packaging, whereas the R1 suffix refers to "tape and reel" packaging.  You are actually comparing the unit price for purchace of a single piece, to that for a reel of 1000 pieces.

 

Regards,

Mac

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,898件の閲覧回数
bigmac
Specialist III

Hello Bob,

 

According to the Freescale website, this part has the classification of "maturity/saturation" which means that it is still active.

The T suffix refers to "tray" packaging, whereas the R1 suffix refers to "tape and reel" packaging.  You are actually comparing the unit price for purchace of a single piece, to that for a reel of 1000 pieces.

 

Regards,

Mac

 

0 件の賞賛
返信
1,897件の閲覧回数
Bobli
Contributor I

mac,

 

I found the information at http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MMA7660FC&tab=Buy_Parametric_Tab&from.... Its "status" is "active", which means this is currently production.

 

"Product maturity" should mean the type is already out of experimental phase and is a mature product.

 

But what does "saturation" mean here?

 

 

Bob

0 件の賞賛
返信