Question about HCS08's FLL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question about HCS08's FLL

Jump to solution
2,183 Views
765208638
Contributor II

Dear everyone & NXP engineers:

   I am very happy to use HC9S08SG to do my job.I have a question about it's FLL(FEE).

In doc《AN3041》,pastedImage_2.png

We can see it is  multiply by 512.

and when useing  PE on CW6.3,as below

pastedImage_3.png

we can see it is multiply by 1024,so i am a bit confused.Maybe i did not read the ducument carefully?

So ,could you everyone please help me about this question.

At lasy ,my english is not good ,please forgive me .

Thanks all.

Tags (1)
0 Kudos
Reply
1 Solution
2,051 Views
john_suchyta
NXP Employee
NXP Employee

Hi. AN3041 applies to the first version of the Internal Clock Source (ICS). You need to check the datasheet for the version that is in the MCU you are using. The SG32 and SG8 MCUs multiply the reference by 1024, as shown in the PE window.

Regards,

John

View solution in original post

0 Kudos
Reply
2 Replies
2,052 Views
john_suchyta
NXP Employee
NXP Employee

Hi. AN3041 applies to the first version of the Internal Clock Source (ICS). You need to check the datasheet for the version that is in the MCU you are using. The SG32 and SG8 MCUs multiply the reference by 1024, as shown in the PE window.

Regards,

John

0 Kudos
Reply
2,051 Views
765208638
Contributor II

Hi John

   I see it ,thanks.

0 Kudos
Reply