Question about HCS08's FLL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Question about HCS08's FLL

ソリューションへジャンプ
2,154件の閲覧回数
765208638
Contributor II

Dear everyone & NXP engineers:

   I am very happy to use HC9S08SG to do my job.I have a question about it's FLL(FEE).

In doc《AN3041》,pastedImage_2.png

We can see it is  multiply by 512.

and when useing  PE on CW6.3,as below

pastedImage_3.png

we can see it is multiply by 1024,so i am a bit confused.Maybe i did not read the ducument carefully?

So ,could you everyone please help me about this question.

At lasy ,my english is not good ,please forgive me .

Thanks all.

タグ(1)
0 件の賞賛
返信
1 解決策
2,022件の閲覧回数
john_suchyta
NXP Employee
NXP Employee

Hi. AN3041 applies to the first version of the Internal Clock Source (ICS). You need to check the datasheet for the version that is in the MCU you are using. The SG32 and SG8 MCUs multiply the reference by 1024, as shown in the PE window.

Regards,

John

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,023件の閲覧回数
john_suchyta
NXP Employee
NXP Employee

Hi. AN3041 applies to the first version of the Internal Clock Source (ICS). You need to check the datasheet for the version that is in the MCU you are using. The SG32 and SG8 MCUs multiply the reference by 1024, as shown in the PE window.

Regards,

John

0 件の賞賛
返信
2,022件の閲覧回数
765208638
Contributor II

Hi John

   I see it ,thanks.

0 件の賞賛
返信