QG8 Hanging on Power Reset when UART accessed

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

QG8 Hanging on Power Reset when UART accessed

2,247件の閲覧回数
jimstevens
Contributor I
I've got a simple application that hangs on power reset.  I'm programming it with the P&E USB Multilink through the debug screen in CodeWarrior.  The target is set correctly.
 
Once I disconnect the P&E and do a power cycle, the chip just hangs.  I'm using LEDs to verify correct operation.
 
However, if I comment out my readData (listed below) function which reads data from the UART, everything will function on a power reset.  I've tried both interrupt based and polling for the UART, and it makes no difference.
 
//=============================================================================
// readData
//-----------------------------------------------------------------------------
//=============================================================================
int readData(void *dataBuffer, int dataBufferSize)
{
int          returnValue = 0;
int   i;
  // If we have a bad data buffer pointer then we fail.
  if(dataBuffer == 0)
  {
     goto EXIT;
  }
  for(i=0;i<dataBufferSize;i++) {
          
   while (SCIS1_RDRF == 0);
     
   ((unsigned char*)dataBuffer)[i] = SCID;
   
   SCIS1_RDRF = 0;      //acknowledge Receiver Full flag
        
  }

  returnValue = 1;
  EXIT:
  return returnValue;
}
 
Is there something about the RX on the UART that would prevent the chip from reseting properly?
 
I also have a TX function in there and it works fine.  So I don't think it's the entire UART.
 
Any help is greatly appreciated.
 
James
ラベル(1)
0 件の賞賛
返信
1 返信

1,048件の閲覧回数
peg
Senior Contributor IV

Hi Jim,

The COP is timing out while waiting for the data???

Disable COP or feed dog in your waiting for data to fill buffer loop.

Regards David

 

0 件の賞賛
返信