QE128 FEE to FEI Mode switching upon XTAL failure

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

QE128 FEE to FEI Mode switching upon XTAL failure

1,481件の閲覧回数
tonyp
Senior Contributor II
Hi all,

I've searched the docs about this and there is nothing related I could find.

I'm interested in knowing what happens when during FEE the crystal fails to oscillate.   Does it automatically switch to FEI (the reset default) or does it completely lock up?  I can catch failure during startup and remain in FEI but what if the failure happens after I have switched to FEE?  Is this topic covered someplace?

TIA



Message Edited by tonyp on 2008-09-05 06:27 PM
ラベル(1)
0 件の賞賛
返信
1 返信

538件の閲覧回数
bigmac
Specialist III
Hello Tony,
 
The QE128 seems to be missing the loss of clock detection available on some devices.  So I guess you would be reliant on COP reset eventually occuring.  The COP timer clock selected would need to be the 1kHz source, rather than the bus.
 
Regards,
Mac
 
0 件の賞賛
返信