QE128 FEE to FEI Mode switching upon XTAL failure

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

QE128 FEE to FEI Mode switching upon XTAL failure

1,480 次查看
tonyp
Senior Contributor II
Hi all,

I've searched the docs about this and there is nothing related I could find.

I'm interested in knowing what happens when during FEE the crystal fails to oscillate.   Does it automatically switch to FEI (the reset default) or does it completely lock up?  I can catch failure during startup and remain in FEI but what if the failure happens after I have switched to FEE?  Is this topic covered someplace?

TIA



Message Edited by tonyp on 2008-09-05 06:27 PM
标签 (1)
0 项奖励
回复
1 回复

537 次查看
bigmac
Specialist III
Hello Tony,
 
The QE128 seems to be missing the loss of clock detection available on some devices.  So I guess you would be reliant on COP reset eventually occuring.  The COP timer clock selected would need to be the 1kHz source, rather than the bus.
 
Regards,
Mac
 
0 项奖励
回复