QD4 EEPROM Emulation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

QD4 EEPROM Emulation

3,933 Views
abicash
Contributor III

Hello

I am trying to write some 70 bytes  into the flash of QD4 during run time.

I have 256 bytes of RAM, most of it is allocated. Although can spare a good amount for stack.

What do you think is the chance of achieving this in such kind of setup?

 

I understand that Flash erase and Write functions have to be copied in RAM and run from there.

Further I am intending to compare this block of data (written as a constant in Flash)  with actual data arriving in RAM.

 

I need to know the feasibilty for this with 256 bytes on hand.

I really dont have any other choice than QD4,so can't use other devices.

Please provide some comments/pointers/anything as usual.

 

Thanks and regards

Labels (1)
0 Kudos
Reply
5 Replies

2,498 Views
celsoken
Contributor V

Dear Abicash,

 

I remember that DoOnStack has a small footprint and maybe it suits your application.

If you cannot find the updated version I can send you a 4-yr old QG8 implementation.

 

Cheers,

 

Celso

0 Kudos
Reply

2,498 Views
abicash
Contributor III

Hello celsoken

 

Thanks for reading and replying .Much appreciated :smileyhappy:

 

Yes I found the things...And I wrote the code.

 

But I am finding a problem of stack and the data overwriting themselves.

 

I have to sacrifice around 50 bytes for Flash writing and erasing.Is your code in RAM lesser than this?

 

If it is then I would love to see the code.

 

Thanks and regards

0 Kudos
Reply

2,498 Views
celsoken
Contributor V

Dear Abicash,

 

Sorry but I just saw your message, sometimes my email server deletes non-spam msgs.

I am not sure about the footprint, but it could come close to your 50 bytes, anyway it is far beyond 10-bytes Mac´s solution.

 

Cheers,

 

Celso

0 Kudos
Reply

2,498 Views
abicash
Contributor III

Hello Celso and Bigmac

 

Thank you both for your interest in my problem.Much appreciated.

 

As usual Bigmac is the 'Man of Miracles' :smileyvery-happy:

 

I have only seen the code that Bigmac's talking about.

 

I will implement it soon.Only editing prm file will do with Bigmac's code?

 

Although I have been able to run my existing code with a little modification to

 

my prm file and i don't have any overwriting now.

 

Thanks and regards..

 

 

0 Kudos
Reply

2,498 Views
bigmac
Specialist III

Hello,

 

The following recent thread may be of interest -

http://forums.freescale.com/freescale/board/message?board.id=8BITCOMM&thread.id=13469

 

The RAM requirement is 10 bytes for the RAM resident function.  The code shown is for QG8, but could be adapted for QD4.  The RAM function is copied from flash, starting at the bottom of the stack, with the stack pointer  initialised to the top of RAM.

 

Regards,

Mac

0 Kudos
Reply