Protel library for the MC9S08GT60CFB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Protel library for the MC9S08GT60CFB

3,388 Views
Shankman
Contributor II
Does anyone know if the MC9S08GT60CFB has a protel library? So i can design a circuit.

Regards

Kris
Labels (1)
0 Kudos
Reply
2 Replies

1,056 Views
djmoore
Contributor I
Its very easy to create a symbol and footprint in Protel/Altium
Designer, you should try to take the time to learn how, as you
will often need to create new components. You could start with
a part that is close to what you need and make a copy then edit
that.

Regards,
Darren Moore
0 Kudos
Reply

1,056 Views
mjcoury
Contributor I
I believe you just have to start with a default package that matches the specific chip? Protel should have all the default packages in the library already. Then you need to look up the particular chip package you are using, that nugget of info is in the datasheet for the chip... add the lables and save it in the library as a new part and you should be good!
0 Kudos
Reply