Programming MC68HC908QY4A

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Programming MC68HC908QY4A

1,543 Views
madhub
Contributor I

Dear all,

 

 Is it possible to loas s-record into flash of the QY4A without using usb-Mon-08 from P&E or cyclone pro.

 

Is it possible to use monitor mode entry ckt available in datasheet to program the flash of controller.

 

The security feature is very confusing in it.It says that to load data into flash the security bits has to be entered into flash

 

locations FFF6-FFFD,but these locations are ISR vector addresses.Please some could clarify on these things.

Labels (1)
0 Kudos
Reply
1 Reply

1,215 Views
peg
Senior Contributor IV

Hello and welcome to the fora madhub.

 

Yes this is possible.

To get past security you must send the same value as is programmed into these vector locations at the appropriate time.

You can get a free programme to do this from here.

 

0 Kudos
Reply