Programming Flash on AC128

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Programming Flash on AC128

2,372件の閲覧回数
Davo
Contributor II

Hi,

I am building an app using the AC128.  I ported the flash programming routines I craeted for a previous app on a QG8, but they didn't work.  I notice a few changes to the flash programming registers, e.g. FOPT, but after correcting these the routines still don't work.

 

Any thoughts appreciated on the variations to the AC128 flash programming model before I get head down into the debugging phase.

 

David

ラベル(1)
0 件の賞賛
返信
1 返信

1,446件の閲覧回数
Davo
Contributor II
Just picked-up this project again after a long break.  I'm still unable to program flash on the AC128 using the routines I have previously used on the QG8 and SH8. The processor resets when I attempt to write to flash. Any thoughts would be appreciated on any major differences with the AC128 that I may not have noticed.
0 件の賞賛
返信