Programing "High-end" microcontrolers with USBSPYDER08

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Programing "High-end" microcontrolers with USBSPYDER08

2,625件の閲覧回数
admin
Specialist II
Hi

I have bought a USBSPYDER08 kit and I would like to use the BDM interface to program the better microcontrolers (for example AW60 etc.). But in CodeWarrior It's possible to chose QD4, QG4 and QG8 only. So i would like to ask you. It's possible to add another microcotroler or does exist "better" drivers for USBSPYDER08?

Thank You for Answer
ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,062件の閲覧回数
SBrazz
Contributor I
0 件の賞賛
返信

1,062件の閲覧回数
peg
Senior Contributor IV
Hi Mica,
 
I was wondering about this too when I saw it come out.
I don't have an answer for you but I suspect there is some deliberate "hobbling" going on here in order to protect sales of higher end adapters.
I would like to know the technical reasons behind this limitation as well. There is very little difference between supporting a QG and a GB or AW.
 
0 件の賞賛
返信

1,062件の閲覧回数
joerg
Contributor II
Hi
that is the fine thing of low cost development systems; when you see your device is to weak for your application you have to switch to a bigger environment. You then not only have to install the software again, your hardware is also obsolete!
For this reason i prefer a modular design. A long, long time ago i have begun to build up my modular development system. First based on the ECB-Bus (CP/M80, Z80) and later my own "standard". This includes a port connector with the bits always on the same location as well as some power pins for powering the "addons". I am now able to switch between different MPU's by changing the MPU module. That works for the HCS08, HC08 and RS08 family, even the software can be modified thanks to EBS08!
I am wondering why the whole word is designing EVB's for a single MPU (a lot of repeated work for layouting and testing) with solder pads on it (they are looking ugly after a short time!!), when it could be done much easier.

The first pic is showing a GB32 module with the baseplate and two RS232 converters while testing the software for a milling machine and the second pic is the KAx module with the OSBDM+E and the porttester during EBS08R testing.

Saluti Joerg
0 件の賞賛
返信